Dock a graphic object
Anchor graphic objects in the window by docking the object.
Dock objects on any side of the window while maintaining margins, in the center while resetting margins, or stretch graphic objects across a container.
- InProject view, double-click a container or select.The editor opens in a separate tab.
- In the editor, select the graphic objects to anchor. To select multiple graphic objects, hold downCtrland select additional graphic objects.
- In the editor toolbar, select the button to dock the graphic object:
- Dock left. Anchor the selected objects the left while maintaining margins.
- Dock right. Anchor the selected objects on the right while maintaining margins.
- Dock top. Anchor the selected objects at the top while maintaining margins.
- Dock bottom. Anchor the selected objects at the bottom while maintaining margins.
- Dock center. Anchor the selected objects vertically while centering the objects and resetting margins.
- Dock center. Anchor the selected objects horizontally while centering the objects and resetting margins.
- Dock left and right. Stretch the selected objects horizontally across the container.
- Dock top and bottom. Stretch the selected objects vertically across the container.
Provide Feedback