Move a graphic object

Move a graphic object

Move a graphic object in the window to position objects as they will appear at runtime. All of the objects in a container move with the container.
  • To move a graphic object either:
  • In the window, select and drag the container or graphic object.
  • In
    Project view
    , select the container or graphic object and then in
    Properties
    change:
    • Horizontal alignment
      . Enter the value for the space between the object and the X-axis.
    • Vertical alignment.
      Enter the value for the space between the object and the Y-axis.
    TIP: The position of the graphic object in
    Project view
    determines the order of graphic objects on the Z-axis compared to other objects in the same container. Objects lower in the tree appear higher in the order on the Z-axis.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal