Create a Presentation Engine
Add a Native Presentation Engine or a Web Presentation Engine to your project.
TIP:
Each project can contain a single Native Presentation Engine and a single Web Presentation Engine.
- InProject view, right-click a window object.
- Select one of the following options:
- To create a default Presentation Engine, select.
- To create a Web Presentation Engine, select.
- InProperties, set any required Presentation Engine properties.
Provide Feedback