Use an existing style sheet

Use an existing style sheet

Use a predefined style sheet. You can also create and configure a custom style sheet.
  1. Select
    Template Libraries
    .
  2. In
    Libraries
    , select
    StyleSheets
    to open the style sheets in the project.
  3. Drag the desired style sheet into the
    UI
    folder of
    Project view
    .
Graphic objects located under the folder that contains the style sheet in
Project view
now inherit the styles configured in the style sheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal