Commit a library
Commit changes to a local or remote library to save changes on the local computer only. Committed changes are not backed up (or pushed) to a remote repository.
Prerequisites
- To commit a library
- From the main toolbar, select.Template Libraries
- SelectCommit.
- Enter a meaningful commit message.
- SelectOK.
A new version of the library is saved on the local computer.
Provide Feedback