Create a library folder
Create a folder in a local or remote library to organize the templates that belong to that library.
- From the main toolbar, select.Template Libraries
- Select a library in which you want to add a folder.
- InTemplate Libraries, selectand selectNew folder.
- (optional) Enter a name for the folder.
New folder appears under the selected library in
Template Libraries
.Provide Feedback