Apply a template
Place a template in a node in
Project view
so that objects in the node can use the template.
TIP:
If the template is a graphic element, you can drag the graphic element from the library into the editor.
- From the main toolbar, selectTemplate Librariesand then either:
- Drag a template from the library into a node inProject view.
- Drag a template that is a graphic element fromLibrariesinto the editor.
Provide Feedback