Deadband interval configurations

The deadband helps prevent sampling values in rapid succession due to oscillation in the control system.
Sampling type
Deadband settings
Any change from the previous sample
Default deadband mode
=
None
Absolute value of change from the previous sample is equal to or greater than a specific value
  • Default deadband mode
    =
    Absolute
  • User-specified
    Default deadband value
Percentage of change from the previous sample is equal to or greater than a specific value
  • Default deadband mode
    =
    Percentage
  • User-specified
    Default deadband value
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.