Store read operation codes
Configure the logger to store the operation codes of reading on the controller in the database.
TIP:
For more information about the read operation codes, see Read operation codes.
Prerequisites
- To store read operation codes
- InProject view, select a data logger object.
- InProperties, setLog operation code of each variabletoTrue.
Provide Feedback