Add a locale language to a localization dictionary
Add locale languages to a localization dictionary so you can change the language displayed for an application at runtime.
- InProject view, expandTranslationsand double-click a localization dictionary.
- In the localization dictionary, in theTranslation tableview, selectAdd locale.
- UnderSelect the new locale, select a locale language and then select.
- InNew locales added, to add the locale to the displayed objects, selectYes.
A new column appears for the locale.
Provide Feedback