- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Change the interface language
Change the interface language to display a different language throughout the
FactoryTalk Optix Studio
application at design time and runtime. - To change the interface language, either:
- InProject view, select the project node and then inProperties, expandLocalizationand inLocales, select the language.
- Selectand then inFactoryTalk Optix Studio OptionsLanguage and Locale, select the language.
- Have a different user with a different associated locale language log on.
Provide Feedback