Edit an enumeration
Edit members of an existing enumeration object.
- InProject view, double-clickEnumeration.#Enumeration editor displays in the central pane.
- In the editor, manage the enumeration members:
- To add a member, selectand complete:
- Value. Enumeration member value. Value is generally a consecutive integer.
- Display name. Name of the enumeration member.
- Description. Additional information about the enumeration member.
- To edit aValue,Display name, orDescription, double-click the corresponding cell and enter a new value.
- To remove a member, select a cell in the corresponding row and select.Delete
Provide Feedback