Create an object
Create an object to add the node to
Project view
.- InProject view, select the folder in which to create the object and then selectin theProject viewtoolbar, or right-click the folder and selectNew.The context menu that appears displays objects that the folder can contain based on the folder category.
- SelectObjector the specific object.
ObjectName1
appears in Project view
.Provide Feedback