Create a variable
Create a variable in
Project view
.- InProject view, select the folder or object to contain the variable.
- In theProject viewtoolbar, selectAdd newand then selectVariable.
- (optional) To change the variable data type, inProperties, next to the variable name, select the existing data type and then select another data type.TIP: If you do not see the required option, selectShow all. To define an array, selectArrayand then enter the array dimensions.
- InProperties, enter a value for the variable or create a dynamic link.For more information about dynamic links, see Create dynamic links.
- (optional) Set the unit of measure for a variable.
- (optional) Add a range to a variable.
Provide Feedback