OPC UA
FactoryTalk Optix Studio
is compliant with the OPC UA (OPC Unified Architecture) standard and can communicate with any OPC UA client or server.
TIP:
Devices with a configured
FactoryTalk Optix Application
can operate as an OPC UA client or server.Use these components to develop your application logic:
- OPC UA server object
- OPC UA client objects
- OPC UA nodes
Provide Feedback