- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create a report
Create a report by adding the report to
Project view
. Configure and add components to the change the appearance of the report.
- InProject view, right-clickReportsand then select .TheReports#appears inProject view.
- InProject viewafter the report or inPropertiesafterName, selectto enter a meaningful name for the report.TIP: To change the format of all of the pages in the report, with the report object selected inProject view, edit the variables inProperties. Global properties affect all pages in the PDF output.
- InProject view, expand the report.
- Select theHeaderobject and edit the values inPropertiesto change the appearance of the header.
- Add panel sections to the report:
- InProject view, right-clickSectionsand select .
- SelectPanelSection#and edit the values inPropertiesto change the appearance of the panel section.
- Add a data grid section:
- InProject view, right-click theSectionsobject and select .
- SelectDataGridSection#and edit the values inPropertiesto change the appearance of the data grid section.
- To add a page break, inProject view, right-click theSectionsobject and select .
- Select theFooterobject and edit the values inPropertiesto change the appearance of the footer.TIP: To design the user interface of the header, panel section, data grid section, or footer, expand the report inProject viewand then double-click the object to edit the object in the editor for the object.
Provide Feedback