Configure measurement systems map
Use preferred engineering units in unit systems associated with project locales. Map custom units in these systems: International System of Units, US Customary Measurement System, British Imperial Units.
TIP:
The session locale determines the measurement system for the displayed data. For example, a session with the en-US locale displays temperatures in Fahrenheit degrees.
Prerequisites
(optional) Define custom engineering units. See Create an engineering units dictionary.
- To configure measurement systems map
- InProject view, select the project root node.TIP: The root node is at the top ofProject viewhas the same name as your project.
- InProperties, next toMeasurement systems map, selectEdit with Measurement system editor.
- To add a measurement systems map row, select.
- To edit a measurement systems map row, hover-over a cell, select the drop-down arrow, and select a value.Fromindicates the input quantity of interest or the value from the sensor to be converted. The selected units of measure will be translated to the equivalent quantity for the different locales in these columns:
- International System of Units
- US Customary Measurement System
- British Imperial Units
- (optional) To delete a measurement systems map row, select a cell in the measurement systems map row and select.Delete
From | International System Of Units | US Customary Measurement System | British Imperial Units |
---|---|---|---|
Volume: liter [l] | liter [l] | quart (US) [qt (US)] | quart (UK) [qt (UK)] |
Provide Feedback