Time zones for alarm events
At runtime, the
Data grid
object of the Alarm grid
and Alarm log grid
objects display the local time of events in the Timestamp
column: Object | Timestamp |
---|---|
Alarm grid | Set a dynamic link in the Time property. |
Alarm history grid | Set a dynamic link in the Time property with a node pointer. |
In projects that support remote sessions, devices with different local time settings can display different time zones in the widgets. The timestamp of the widget displays in the local time zone of the device, even when events occur in different time zones. In the
Timestamp
column of the Alarm grid
or Alarm history grid
, set a converter of type Expression evaluator
with the sum of the properties {Item}Time
and {Session}TimeZoneOffset
. See View alarms in remote local time zone.Provide Feedback