Create a button to restart the application
You must restart the
FTOptixApplication
to have any date and time changes from the Date and time configurator
widget take effect. Create a button to restart the
FTOptixApplication
.- InProject view, right-click the folder to contain the button and select .Button# (type)appears inProject view.
- WithButton# (type)selected, inPropertiesunderEvents, selectAdd new methodnext to the event, such as aMouseClick event, that you want to close theFTOptixApplication.
- ExpandCore commands, selectRestart, and then chooseSelect.
Provide Feedback