Assign a group to a user
ssign groups and create a hierarchy of rights and privileges.
- In the main toolbar, either:
- Select, and then on the dashboard, selectOpen dashboard pageManage users and groups.
- Select the drop-down arrow after, and then selectOpen dashboard pageManage users and groups.
- In the editor, either:
- From underGroups,drag a group onto a user or hold downShiftorCtrlto select and drag consecutive or multiple groups to a user.
- Select the checkbox of one or more groups, selectAssigngroups to users, select the checkbox of a user, and then selectApply.
appears next to a user that is already assigned to a group. - SelectExit.
- Select.SaveIn the editor, you can drag a user into a group.
Provide Feedback