Add a user
Add users to
Project view
. Manage existing users by adding them to groups and giving them permissions. - InProject view,expandSecurity.
- Right-clickUsersand then select .User#appears.TIP: To add users, you can also right-clickUsers, and then select .
- InProperties,configure:
- Name. Name of the user.
- Password. Password that the user must provide to log on to the application.
- LocaleIds. Locale of the user. The default is en-US.
- Languages. Language configured for the user. The default language is the default language of the LocaleId.
- Measurement system. The measurement system used to display data to the user:
- International system of units
- US customary measurement system
- British imperial units
- Domain. Identifies the localWindows®user account for any domain-linked user account.
- Select.Save
Provide Feedback