Add version control to an existing project

Add version control to an existing project

Add version control to an existing project that either has no active version control, or a remote repository that does not have the supported
GitHub®
version control system. Projects without version control do not display icons to commit, push, or pull changes or to version history. You can version projects externally using tools provided by a supported version control provider.
To add version control to an existing project
  1. With the project open, in the main toolbar bar, select the drop-down arrow after
    Save
    and then select
    Save As
    .
  2. In
    Save project as
    , enter:
    • Name
      . The name of the project. Use the same name as the remote repository.
    • Location
      . The folder to contain the project.
    • Use Version Control
      . Select to add version control to the project.
      TIP:
      If the project already has version control and
      Use Version Control
      is already selected,
      FactoryTalk Optix
      creates a new local repository for the project without any previous commit history.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.