Configure version control
Version control is required to version projects that you create. Each project uses version control by default.
If you already use version control on your computer, version control is automatically configured in
FactoryTalk Optix Studio
. If you are not already using version control on your computer, configure version control in FactoryTalk Optix Studio
.- In the title bar, select.FactoryTalk Optix Studio Options
- SelectVersion control.
- UnderVersion Control User Configuration, inUser Name, type your username.TIP:User Nameis the name that appears next to commits when you openView historyfor a project. View history also identifies your commits with an avatar that uses the first letter of your name.
- InUser Email, type your email address.
- SelectSave.
Provide Feedback