Create a dynamic alarm message

Create a dynamic alarm message

Create an alarm message that appears at runtime when the alarm is active. For example, create a message that indicates a flow rate or level is dangerously low when the alarm is active.
Prerequisites
  1. To create a dynamic alarm message
  2. In
    Project view
    , select the alarm.
  3. In
    Properties
    , in
    Message
    , select
    Add Dynamic Link
    , and then select
    Advanced
    .
  4. In the
    Dynamic Link Editor
    , in
    Message
    , select
    Add
    and then select
    String formatter
    .
  5. In
    Dynamic Link
    , select
    Change Dynamic Link
    .
  6. Specify the
    Input value
    of the alarm as the source for the Dynamic Link.
  7. In
    Format
    , enter the text of the alarm message, using the placeholder
    {0}
    to identify the value of the source variable.
  8. Select as necessary to set the direction of the link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.