- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Set dynamic variables polling time for alarms
Set the time interval between readings of variable values from OPC UA servers and tag values from controllers.
- InProject view, select the root project node.
- InProperties, setDynamic variables polling time.TIP: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.
Provide Feedback