Expression evaluator
Calculate the result of an expression with integers, decimals, numeric variables, string variables for string comparisons, arithmetic and Boolean operators, or a set of functions.
Properties
Property | Description |
---|---|
Expression | The expression to be calculated. The expression can contain an unlimited number of correctly opened and closed parentheses. If the expression does not follow the correct syntax, the converter will not perform the calculation. |
Mode | The direction of the dynamic link:
|
Source
One or more variables, identified by a placeholder with an index number in the following format {index}. The index number is progressive, must be an integer greater than zero {0}.
The placeholders can appear in any order in the expression.
Valid literal values
- Boolean true and false.
- Integers.
- Decimals where the decimal separator must be a point.
- Hexadecimal numbers with the prefix "0x".
- Text such as a string delimited by double quotation marks.TIP: Double quotation marks repeated twice ("") are interpreted as an escape sequence.
Valid operators
- Arithmetical:+,-,*,/,%, and the unary operator-
- Bitwise:&,|,^,~
- Shift:<<,>>
- Logics:&&,||,!
- Unary casting of(<data_type>)type
- Comparison<,<=,>,>=,==,!=NOTE:The comparison operators apply to:
- The numeric data
- DateTime data
- Duration data
The operators:==and!=also apply to String and LocalizedText data types.
Data type conventions
- Literal integers areInt32.
- Decimal literals areDouble.
- Numerical values are considered to beInt32.
- Literals true and false are interpreted asBoolean.
- The / operator always returns aDoublevalue.
- The % operator generates an exception when there is division by modulo zero.
- The % operator acceptsFloatandDoubleoperands.
- All functions return aDoublevalue except for sign, which returns anInt32value.
- The unary casting operator accepts data types:
- bool, Boolean
- sbyte, SByte
- short, Int16
- int, Int32
- long, Int64
- byte, Byte
- ushort, UInt16
- uint, UInt32
- ulong, UInt64
- float, Single
- double, Double
Available functions
The following mathematical functions are available:
Function | Calculated value | Example |
---|---|---|
max | Maximum of two values. | max ({0}, {1}) |
min | Minimum of two values. | min ({0}, {1}) |
avg | Average of given values. | avg ({0}, {1}) |
abs | Absolute value. | abs ({0}) |
trunc | Integer part of a decimal number. | trunc ({0}) |
ceil | Approximated value by excess. | ceil (({0} + {1})/2) |
floor | Approximated value by defect. | floor (({0} + {1})/2) |
round | Approximation to the nearest integer. | round (({0} + {1})/2) |
sqrt | Square root. | sqrt ({1}) |
sign | 0 if the argument value is greater than zero.1 if the argument value is less than zero. | sign ({1}) |
Output
The resulting value of the expression.
Example

Provide Feedback