Linear converter

Linear converter

Convert raw data values into scaled values based on the linear relationship applied to the input.

Properties

Property
Description
Slope
Steepness of the line.
Intercept
The point on the Y-axis through which the slope of the line passes.
Mode
The direction of the dynamic link:
  • Read from the source node to the parent.
  • Write from the parent to the source node.
  • Read from the source node to the parent and write from the parent to the source node.

Source

A variable that contains a raw value to be converted.

Output

A scaled value based on the configured linear conversion.

Example

Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.