Duplicate a client device

Duplicate a client device

Duplicate a client device to configure another similar client device.
  1. From the main toolbar, next to
    Run
    , select the client dropdown menu.
  2. (optional) In
    Client device settings
    , to display only the active remote client devices, toggle
    Active remote devices
    .
    TIP: Refresh remote client devices by selecting
    Refresh
    .
  3. Select a client device.
  4. Select
    Duplicate
    .
Configure the duplicated client device properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.