- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Project encryption
Encrypt projects on
Windows®
client devices and OptixPanel™
.Encryption scope
Project
YAML
files, which represent the project information model, are transferred as encrypted binary files on client devices. For more information, see Project source format.By default, Emulator components are encrypted. You cannot disable the encryption of Emulator components.
Public encryption key
Client devices generate public encryption keys based on the current hardware and
Windows
keys. The public encryption keys in EncryptionKey.bin
are stored on the client devices in the Runtime
folder.Encrypted projects cannot be copied to or run on different client device.
Provide Feedback