Remove a client device
Remove client devices that you no longer need.
- From the main toolbar, next to, select the client dropdown menu.Run
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select a client device.
- SelectRemove the selected target device.
- In theClient device settings, selectRemove.
Provide Feedback