Create a complex dynamic link

Create a complex dynamic link

Create complex dynamic links to transform linked values.
  1. In
    Project view
    , select an object that contains a property to link.
  2. In
    Properties
    hover-over the property to link, select
    Add Dynamic Link
    .
  3. In the dynamic link browser, select
    Advanced
    .
  4. (optional) To open the complex dynamic link editor in the central pane, select
    Open in editor
    .
    TIP: Opening the complex dynamic link editor in the central pane is useful if you edit a complex dynamic link with a lengthy logic.
  5. To insert a dynamic link:
    1. Select
      Insert
      and select
      Dynamic link
      .
    2. Set the dynamic link source by selecting
      Add Dynamic Link
      or dragging and dropping an object or a property.
      The reference to the selected node or variable appears in the property. Before the property, appears to indicate that the property contains a dynamic link.
      TIP: If the dynamic link does not resolve at design time, appears before the dynamic link. A dynamic link to a Windows alias may resolve at runtime. If the dynamic link is broken because the linked attribute no longer exists or has been moved, appears before the link.
  6. To insert a converter:
    1. Select
      Insert
      and select a converter.
    2. Create the converter logic by entering data or creating dynamic links in the converter fields.
      TIP: You can create a dynamic link by selecting
      Add Dynamic Link
      or dragging and dropping an object or a property.
  7. To change the dynamic link direction, select the icon:
    • Read from the source node to the parent.
    • Write from the parent to the source node.
    • Read from the source node to the parent and write from the parent to the source node.
  8. To link the source variable to the specific index of the parent variable:
    1. Select
      Configure
      Configure
      and select
      Add parent array index
      .
    2. Set
      Parent array index value
      .
  9. To create a converter on which you can dynamically build the variable source path, select
    Configure
    Configure
    and select
    EU Mode
    :
    • Default
      . No conversion is applied.
    • Localize
      . Sets the unit of measure of the parent variable based on the user locale.
    • Copy EU from source
      . Sets the unit of measure of the parent variable as the unit of measure of the source variable.
  10. To add a dynamic path converter:
    1. Select
      Configure
      Configure
      and select
      Key-value converter
      or
      Conditional converter
      .
    2. Set the converter properties.
  11. To delete a dynamic link or a converter, in the block, select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.