Add users

Add users

Add users with different locales.
Prerequisites
  1. To add users
  2. In
    Project view
    , expand
    Security
    .
  3. Create two users by right-clicking
    Users
    and selecting
    New
    User
    .
  4. Rename the users by hovering-over each user, selecting
    Edit
    , and entering:
    • Alice
    • Jeremy
  5. In
    Project view
    , select
    Alice
    .
  6. In
    Properties
    , set
    LocaleIds
    to
    it-IT
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.