Delete a method from an event
Delete a method from an event to no longer have the event perform that method.
Delete all of the methods from an event to delete the event.
- InProject view, select an object.
- InPropertiesunderEvents, expand the event.
- After the method to delete, select.Delete
The method is removed from the event.
Provide Feedback