Graphic objects layout

Graphic objects layout

The layout of a user interface for a
FactoryTalk Optix Application
depends on the elements defined for each of the graphic object components.
When creating the user interface, consider how these items will affect your application:
  • Size
    . The size and aspect ratios of the screens on which the interface will be displayed.
  • Position
    . The alignment and margins of the objects with respect to the width and height properties of the objects.
  • Order
    . The relative position of objects to each other within the interface and as implied by the information model of the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.