Checkbox
Sets and displays a Boolean value using select and clear.
Operation
- Selected checkbox
- The associated variable value is True.
- Cleared checkbox
- The associated variable value is False.
Use case
Enable or disable functions or features within a
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.Example
Cleared checkbox
![animated graphic showing selecting and clearing a Checkbox](/content/dam/dita/en/factorytalk-optix/1-2-0/_images/ref_checkbox_ex.png/_jcr_content/renditions/original)
Selected checkbox
![animated graphic showing selecting and clearing a Checkbox](/content/dam/dita/en/factorytalk-optix/1-2-0/_images/ref_checkbox_ex2.png/_jcr_content/renditions/original)
Provide Feedback