Horizontal layout

Horizontal layout

Panel that automatically arranges objects horizontally next to each other.

Use case

Lay out interface elements horizontally. For example, lay out buttons or other objects.
TIP: To achieve a different order of the interface elements, arrange the objects in the model.

Example

The positioning and distance between the buttons depend on the margins set on these buttons.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.