Vertical layout
Panel that automatically arranges objects vertically next to each other.
Use case
Lay out the graphic elements vertically. For example, lay out buttons or other objects.
TIP:
To achieve a different order of the interface elements, arrange the objects in the model.
Example
The positioning and distance between the buttons depend on the margins set on these buttons.

Provide Feedback