Navigate a trend chart

Navigate a trend chart

Navigate the X-axis and Y-axis of a trend chart.
  • Select a point and drag it horizontally to navigate the X-axis.
    TIP: If the
    Follow
    property is set to
    True
    , automatic scrolling stops when you interact with the graph. To restart the automatic scrolling of the X-axis, scroll the X-axis to the current instance.
  • Select a point and drag it vertically to navigate the Y-axis.
  • Select a pointer and drag it diagonally to browse on both axes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.