Advanced SVG image

Advanced SVG image

Use this object to display an SVG Tiny 1.2 image and change the properties of individual image parts at design time or runtime.
Application example - disabled alarm
Application example - enabled alarm

Use case

Statically or dynamically modify a part or the entire SVG image. For example, signal a hardware part malfunction by highlighting a given hardware component representation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.