Draw a line

Draw a line

Use the
Line
tool to draw a line.
  1. In
    Project view
    , double-click the container to include the object.
  2. In the editor toolbar, select
    Line
    .
  3. In the editor, position the crosshair where the line, polyline, or polygon is to begin.
  4. Drag to draw the line.
The object appears in the editor and in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.