Draw a rectangle or square

Draw a rectangle or square

Use the
Rectangle
tool to draw rectangles or squares.
  1. In
    Project view
    , double-click the container to include the object.
  2. In the editor toolbar, select
    Rectangle
    .
  3. In the editor, position the crosshair where the square or rectangle is to begin.
  4. Drag to draw a rectangle or square.
The object appears in the editor and in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.