Edit an image
Edit an image on the canvas to edit the picture that appears in the image object.
- FromProject view, double-clickMainWindow (type)to open the editor in a separate tab.
- On the canvas, double-click the image you want to change.NOTE: You can also edit an image fromProject viewby double-clicking the image inProject viewto open a tab in the editor.
- InSelect file, select the image to display and then chooseSelect.TIP: If the image does not appear inSelect file, selectand inImport file(s)Import file(s), select the image to import and then chooseSelect.
Provide Feedback