Configure a presentation engine
Add a native presentation engine or a web presentation engine to your project.
TIP:
Each project can contain a single native presentation engine and a single web presentation engine.
- InProject view, right-click a window object.
- Select one of the following options:
- To create a native presentation engine, select.
- To create a web presentation engine, select.
- (optional) InProperties, edit the presentation engine options.
Provide Feedback