Create elements for controlling the current value

Create elements for controlling the current value

Create a gauge and other interface elements that display the current value and enable you to edit it.
  1. Create the current value label:
    1. In
      Project view
      , right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over a gauge, select
      Edit
      , and enter
      CurrentValueLabel
      .
    3. In
      Properties
      and set
      Text
      to
      Current Value
      .
  2. Create the value gauge:
    1. Right-click
      MainWindow (Type)
      and select
      New
      Base controls
      Linear gauge
      .
    2. Hover-over a gauge, select
      Edit
      , and enter
      ValueGauge
      .
    3. In
      Properties
      , create a dynamic link between the
      Value
      and
      ProjectName
      Model
      ConstrainedVariable
      .
      For more information about dynamic links, see Create dynamic links.
  3. Set the value gauge warning zone 1:
    1. In
      Properties
      , next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone1
      , set
      Color
      to
      #f30000
      .
    3. Create a dynamic link between
      From
      and
      ProjectName
      UI
      MainWindow (Type)
      ValueGauge
      Minimum value
      .
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between
      To
      and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      Low limit
      .
      For more information about dynamic links, see Create dynamic links.
  4. Set the value gauge warning zone 2:
    1. Next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone2
      , set
      Color
      to
      #02d92d
      .
    3. Create a dynamic link between
      From
      and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      Low limit
      .
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between
      To
      and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      High limit
      .
      For more information about dynamic links, see Create dynamic links.
  5. Set the value gauge warning zone 3:
    1. Next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone3
      , set the
      Color
      property value to
      #f30000
      .
    3. Create a dynamic link between
      From
      and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      High limit
      .
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between
      To
      and
      ProjectName
      UI
      MainWindow (Type)
      ValueGauge
      Maximum value
      .
      For more information about dynamic links, see Create dynamic links.
  6. Create the value label:
    1. In
      Project view
      , right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over a gauge, select
      Edit
      , and enter:
      ValueLabel
      .
    3. In
      Properties
      , create a dynamic link between
      Text
      and
      ProjectName
      Model
      ConstrainedVariable
      .
      For more information about dynamic links, see Create dynamic links.
  7. Create the value spin box:
    1. In
      Project view
      , right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Spin box
      .
    2. Hover-over a gauge, select
      Edit
      , and enter:
      ValueSpinBox
      .
    3. In
      Properties
      , create a dynamic link between
      Value
      and
      ProjectName
      Model
      ConstrainedVariable
      For more information about dynamic links, see Create dynamic links.
  8. Create the value text box:
    1. In
      Project view
      , right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Text box
      .
    2. Hover-over a gauge, select
      Edit
      , and enter:
      ValueTextBox
      .
    3. In
      Properties
      , create a dynamic link between
      Text
      and
      ProjectName
      Model
      ConstrainedVariable
      For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.