- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Create elements for controlling the max value
Create a label and a gauge to control the maximum value.
- Create the maximum value label:
- InProject view, right-clickMainWindow (Type)and select .
- Hover-over the label, select, and enterMaxValueLabel.
- InPropertiessetTexttoMaximum Value.
- Configure the max gauge:
- InProject view, right-clickMainWindow (Type)and select .
- Hover-over the gauge, select, and enterMaxGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
Provide Feedback