Push a library

Push a library

Push a remote library to a remote Git repository to make the changes available to other users of the remote library.
WARNING: If you use custom
FactoryTalk Optix Studio
or
FactoryTalk Optix Studio
beta, pushing library updates to the remote repository prevents other users from pulling the library if they do not use the same
FactoryTalk Optix Studio
release channel.
  1. To push a library
  2. From the main toolbar, select
    Template Libraries
    .
  3. Select
    Push
    .
  4. If prompted, enter the remote repository URL and user credentials.
    TIP: You can manage the remote repository URL and user credentials in
    FactoryTalk Optix Studio Options
    . For more information, see Configure version control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.