Create a template from an object or variable

Create a template from an object or variable

Use a template to create other objects and variables that have similar attributes.
  1. Select
    Template Libraries
    .
  2. From
    Project view
    , drag the object or variable into a library in
    Template Libraries
    .
    A new template appears under
    Components
    .
  3. (optional) Select the template and enter a description.
    For example, explain how to use or implement your widget.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.