Approve a remote connection from FactoryTalk Remote Access to a device
If you are on a panel and
Approve Remote Access
is enabled in the FactoryTalk Remote Access
application, you may receive requests from FactoryTalk Remote Access
users who are trying to connect remotely to the device. You must then approve or deny a request to connect to the remote device. - On the device, open the screen with theFactoryTalk Remote AccessWidget.If you created your project using the OptixPanel template on the start page, selectSettingsand then selectFT Remote Access
- Connectionson the widget displays theFT Remote Access runtime versionthat is running on the device.A message appears at the bottom of the FT Remote Access widget to either approve or deny the request.
- To allow theFactoryTalk Remote Accessuser to connect to the remote device, selectYesto approve the connection, or selectNoto deny the request.
Provide Feedback