Duplicate a data logger

Duplicate a data logger

Duplicating a data logger configures a new logger based on the existing logger.
  1. From the toolbar, select
    Open dashboard page
    .
  2. In the central pane, select
    Configure a data logger
    .
  3. Right-click the data logger to duplicate and select
    Duplicate
    .
    A new data logger appears in the list of available data loggers.
Edit the duplicated logger settings. See Edit a data logger.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.