- NetLogic tutorial
Configure OPC UA server certificates and keys
Edit the properties of an OPC UA server to configure the public certificates and private keys.
Prerequisites
- To configure OPC UA server certificates and keys
- InProject view, select anOPCUAServerobject.
- InProperties, next toServer certificate file, selectBrowse.
- InSelect file:
- If the certificate is listed, select the certificate and chooseSelect.
- If the certificate is not listed:
- Select.Import file(s)
- Select the certificate. For more information, see Certificates and keys location.
- ChooseSelect.
- Next toServer private key, selectBrowse.
- InSelect file:
- If the private key is listed, select the private key and chooseSelect.
- If the private key is not listed:
- Select.Import file(s)
- Select the private key. For more information, see Certificates and keys location.
- ChooseSelect.
Provide Feedback